Hello,
I'm trying to build a embedded linux image for an am3354 with Yocto fido (tried also jethro) and the meta-ti layer. But I'm stuck when the omap3-sgx-modules are build because of a missing license file.
Error message: Function failed: omap3-sgx-modules: LIC_FILES_CHKSUM points to an invalid file: ../omap3-sgx-modules/5.01.01.02-r00b/Graphics_SDK_5_01_01_02/GFX_LINUX_KM/GPL_COPYING
I ran into the same issue building the libgles-omap3 package. This time the TSPA.txt file is missing.
I noticed that there are some license files in another folder which are called "generic_TI_TSPA" and "generic_GPLv2" but these have different md5 checksums.
Has anyone faced similar issues?
Thx,
Hannes