This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

pspdriver examples on evmOMAPL138 platform build issues.

Other Parts Discussed in Thread: OMAPL138

Hi,

I am working with the pspiom package (pspdrivers_01_30_00) using CCS3 and bios_5_33_05 on the OMAPL138EVM platform. There are several examples that I have tried to build, all with the same two errors:

1. The .tcf file build javascript throws a typeError exception: Can not set property ENABLE of undefined to "1" 

2. Can not open source file "pwrmL138.h"

I must be missing a step, I have looked for similar issues here, but no luck.

Thanks