Hi all,
I'm using ti EVM320C6678LE as my digital signal processor.
I want to load up "led_play.out" from the guide book into the NAND Flash Memory so that whenever I start the DSP with NAND Boot Image 0, I can see User Led flashing.
I've been searching in the forums and guide pdf but just can't seem to find the direct steps in how to load up application into the NAND Flash Memory.
I have tried with the NOR flash memory and it seems to work fine.
Any tips on programming an application in NAND Flash Memory and run it whenever the DSP is turned on?
I'm using CCSv6 in Windows 8.1 64-bit