Other Parts Discussed in Thread: TMS320C5515
Hi,
A redundant perhaps, yet perplexing question that still nags me. Basically the limitation of 64kB of SPI EEPROM for storing application code as noted in the bootloader app note (for the 5505 for instance), is it really the maximum possible ? Is it not possible to "fool" the DSP bootloader into downloading multiple pages of 64kB into the DSP RAM, from multiples sources of SPI EPPROM application code. Has anybody tried this before ? Basically is there really only one option if the code limit of 64kB is reached (which is not much anymore these days), that is to go to SD NAND flash etc. (which basically adds complexity and cost to existing design) ?? Many thanks in advance for your replies.
Cheers, M