This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What could be used as the interface of AM5728 to add one FPGA as co-processor

Other Parts Discussed in Thread: AM5728

Hi,

In order to make the system capable to interface with more video and audio source without compromising the "real time (less burden for the AM5728)", I want to add one FPGA to the system as the multimedia interfaces for the decoders and encoders. I am also planning to use the FPGA to generate the interruption to the AM5728 once the particular data is available.  

Therefore, I am wondering which port I should use as the high speed data transmission interface for the AM5728. 

Any suggestions?

Thanks, Yicheng