This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flashed wrong u-boot.gph image in EVMK2E

Hi Sir/Madam,

I am using EVMK2E v1.0.2.2 board,

I compiled the u-boot.gph image and tried to flash it in SPI-NOR Flash through TFTP server

I did it successfully but problem is I flashed K2H boards configured U-boot.gph image unknowingly.

Because of this I am not getting anything in Minicom/Hyperterminal, no u-boot prompt and nothing.

I can't use CCS to boot U-boot also as the JTAG port in the board have some issues so I couldn't able to connect the CCS

Is there any other method to flash U-boot to the board. Its bloaking as I have to do some testing ASAP

Please provide me with some support to over come this issue.

Thanks & Regards

Sarjoondeen.