Other Parts Discussed in Thread: 66AK2H14, UCD9244, UCD9090, 66AK2H12
Hi
We are developing a PCB based on the 66AK2h14/12/06 (keystone 2) processor rev 2.0 that is similar to EVMK2H. We are having issues in bringing up the DDR2 SODIMM (DDR3A) and DDR3B interfaces. On debug, we can see both interfaces are behaving in the similar fashion. Here is the summary of debug. We can see 100 MHZ clock supplies to SOC (66AK2h14/12/06 )for both DDR3A controller and DDR3B controller are good that is we can see in scope in the input of the SOC is of 100 MHZ frequency and 0.78 V P-P. We are using the same initialization code as provided by TI for EVMK2H that we are running in no boot mode via JTAG emulator. We can see that PLL is get locked but we do not see any clocks coming out of the SoC DDR interfaces and reset remain asserted ~(0 V). We also check the PDSTAT and MDSTAT they are both giving values as 0x301 and 0x10F3, respectively. They seems to be good to us.
Can you please provide us help to figure out why we are not seeing clocks in scope coming out of the DDR interfaces when we think that input DDR’s clocks are good and PLL is locked?
BR
Suresh