This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM648 Reset Problems



Description:

Implement a PC-based Digital Video Recorder,The host may frequently restart the DVR.In the low-lying driver, we will using psc to reset dm648 modules(except PCI) as forllows:

1.Reset C64x+ CPU,by setting MDCTL to 0x000;

2.Restart other modules(except PCI),by setting MDCTL to 0x100 and then 0x103 to bring up them.

3.Config DDR.

4.Bring up C64x+ CPU,by setting MDCTL to 0x100.

5.DSP code download.

6.Set DSPBOOTADDR.

7.Set BOOTCMPLT bit.

System may sometimes hang:

1.DSP can not run.

2.The PSC PTSTAT is always busy.

3.some modules' MDSTAT value is not expected:0x120.

If this happens,I have no way to restart the DSP excpet rebooting my PC.But it is not acceptable.

1.How can i resolve the problem?

2.How can i reset DSP completely,Does PCI-PSC module reset cause completely DSP rest just like POR reset?

 

Best Regards!