Other Parts Discussed in Thread: AM4379
Hi,
We are using am4379 IDK board. We need to connect a FPGA chip using GPMC memory interface.
For AM4379 device datasheet, it is mentioned that the GPMC memory base address starts from 0x00000000 location.it is also mentioned that first 1 MB address space cant be accessible.
We are using CS0. We need around 64MB GPMC memory. To achieve this,what are the values to be set in the following register field?
1) GPMC_CONFIG7_i[5-0] BASEADDRESS bit field.
2) GPMC_CONFIG7_i[11-8] MASKADDRESS bit field.
3) what is the start address that can be used as a first address to read from FPGA device?
Regards,
Jinu