hi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi
Hi,
Thanks for your post.
If you use PAL video, set switch 10 on the S3 (USER) bank of switches to On. If you use NTSC video, set this switch to Off. You can configure the EVM to select either the NTSC or PAL video standard during the default boot sequence too. Kindly refer section 2.1 for setting up the hardware in DM6446 getting started guide as below:
http://www.ti.com.cn/cn/lit/ug/sprue66e/sprue66e.pdf
Kindly see Figure 1–1 which is EVM hardware block diagram for S3 switch bank location on the above doc.
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
--------------------------------------------------------------------------------------------------------