Hi ,
Does AM57xx support big endian?
The EMIF_STATUS register of TRM of AM5728 and AM5718 has the following descriptions.
Table 15-139. EMIF_STATUS
31: BE bit
Big endian mode select for 8 and 16-bit devices, set to 1 for big endian or 0 for little endian operation.
In currentimplementation, only 32-bit devices are supported - this bit is don't care.
This bit is read only.
TRM does not have a mention of the setting of the change of endian of EMIF.
Where is it set?
Best Regards,
Shigehiro Tsuda