Other Parts Discussed in Thread: TLV320AIC3254
Hi,
I'm using a BeagleBone Black running under the latest available Debian and a TLV320AIC3254 evaluation board. I'm struggling to make this codec as an ALSA sound card.
I used the BB-BONE-AUDI-02 DTS file (with a little bit of modification to suit my hardware), the device is found and mounted as an ALSA sound card. I know that the AIC3x is not compatible with the AIC3254.
So I drifted this .dts file to suit my application by replacing tlv320aic3x by tlv320aic32x4 (as the driver seems already available in this linux core). See below.
/* * Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/ * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ /dts-v1/; /plugin/; / { compatible = "ti,beaglebone", "ti,beaglebone-black"; /* identification */ part-number = "BB-BONE-AUDI-02"; version = "00A0", "A0"; /* state the resources this cape uses */ exclusive-use = /* the pin header uses */ "P9.31", /* mcasp0: mcasp0_aclkx */ "P9.29", /* mcasp0: mcasp0_fsx */ "P9.28", /* mcasp0: mcasp0_axr2 */ "P9.25", /* mcasp0: mcasp0_ahclkx */ /* the hardware ip uses */ "gpio1_18", "gpio1_19", "mcasp0"; fragment@0 { target = <&am33xx_pinmux>; __overlay__ { i2c2_pins: pinmux_i2c2_pins { pinctrl-single,pins = < 0x17c 0x73 /*spi0_scl.i2c2_sda,SLEWCTRL_SLOW | INPUT_PULLUP |MODE2*/ 0x178 0x73 /*spi0_d0.i2c2_scl,SLEWCTRL_SLOW | INPUT_PULLUP | MODE2*/ >; }; bone_audio_cape_audio_pins: pinmux_bone_audio_cape_audio_pins { pinctrl-single,pins = < 0x1ac 0x00 /* mcasp0_ahclkx, MODE0 | INPUT */ 0x19c 0x22 /* mcasp0_ahclkr, */ 0x194 0x20 /* mcasp0_fsx, MODE0 | OUTPUT */ 0x190 0x20 /* mcasp0_aclkr.mcasp0_aclkx, MODE0 | OUTPUT_PULLDOWN */ 0x198 0x20 >; }; }; }; fragment@1 { target = <&i2c2>; __overlay__ { #address-cells = <1>; #size-cells = <0>; clock-frequency = <100000>; status = "okay"; pinctrl-names = "default"; pinctrl-0 = <&i2c2_pins>; tlv320aic32x4: tlv320aic32x4@18 { compatible = "ti,tlv320aic32x4"; reg = <0x18>; status = "okay"; }; }; }; fragment@2 { target = <&mcasp0>; __overlay__ { pinctrl-names = "default"; pinctrl-0 = <&bone_audio_cape_audio_pins>; status = "okay"; op-mode = <0>; /* MCASP_IIS_MODE */ tdm-slots = <2>; num-serializer = <16>; serial-dir = < /* 0: INACTIVE, 1: TX, 2: RX */ 2 0 1 0 0 0 0 0 0 0 0 0 0 0 0 0 >; tx-num-evt = <1>; rx-num-evt = <1>; }; }; fragment@3 { target = <&ocp>; __overlay__ { sound { compatible = "ti,da830-evm-audio"; ti,model = "DA830 EVM"; ti,audio-codec = <&tlv320aic32x4>; ti,mcasp-controller = <&mcasp0>; ti,codec-clock-rate = <24000000>; ti,audio-routing = "Headphone Jack", "HPLOUT", "Headphone Jack", "HPROUT", "LINE1L", "Line In", "LINE1R", "Line In"; }; }; }; };
After loading this device tree file, the dmesg differs from the previously pseudo-working file:
[ 249.639414] davinci_evm sound.12: ASoC: CODEC (null) not registered
[ 249.647617] davinci_evm sound.12: snd_soc_register_card failed (-517)
[ 249.662908] platform sound.12: Driver davinci_evm requests probe deferral
When trying to use the ALSA sound card, I get multiple errors such as ALSA lib confmisc.c:768:(parse_card) cannot find card '0'.
I've been looking every relevent forum or website but I couldn't find any applicable or working suggestion. I'm a beginner in beaglebone/linux programming so please be indulgent.
I don't know what can be wrong, any help would be very appreciated.
Thanks