What is this? /////INSTRUMENTATION FOR BATCH TESTING -- Part 1 --  ///// Define PaSs_StAtE variable for catching errors as program executes///// Define PaSs flag for holding final pass/fail result at program completion. Do I need to do this @li Set the PLL frequency to 12.288MHz * @li Run the program and observe the test result * @li Repeat the test at PLL frequencies 40, 60, 75 and 100MHz
 
 Why do I have such trouble in pasteing into this compose post? I copy from example to WordPad to this forum. Martin