This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Building Qt with OpenGL ES on AM335x



hello all ,

i have followed this guide http://processors.wiki.ti.com/index.php/Building_Qt_with_OpenGL_ES_accelerated_by_SGX

am using :

  • Ubuntu   12.0.4 LTS ; 64-bit
  • ti-sdk-am335x-evm-06.00.00.00
  • Graphics_SDK_4_09_00_01
  • qt-everywhere-opensource-src-4.8.2
  • arm-linux-gnueabihf

but i faced many obstacles .

after i run this patch -p1 < 0001-wsegl2-support.patch

i couldn't be able to run this command ./configure from Qtopia that is ti sdk; so i installed Qt everywhere

and started all over again

its all goes will until i reached this command:

./configure -prefix /media/rootf/usr/lib -embedded arm -platform qws/linux-x86_64-g++ -xplatform qws/linux-TIarmv7-sgx-g++ -opengl es2 -plugin-gfx-powervr -D QT_NO_QWS_CURSOR -D QT_QWS_CLIENTBLIT

it run like below :

Which edition of Qt do you want to use ?

Type 'c' if you want to use the Commercial Edition.
Type 'o' if you want to use the Open Source Edition.

o


You have not explicitly asked to use pkg-config and are cross-compiling.
pkg-config will not be used to automatically query cflag/lib parameters for
dependencies


This is the Qt for Embedded Linux Open Source Edition.

You are licensed to use this software under the terms of
the Lesser GNU General Public License (LGPL) versions 2.1.
You are also licensed to use this software under the terms of
the GNU General Public License (GPL) versions 3.

Type '3' to view the GNU General Public License version 3.
Type 'L' to view the Lesser GNU General Public License version 2.1.
Type 'yes' to accept this license offer.
Type 'no' to decline this license offer.

Do you accept the terms of either license? yes

Creating qmake. Please wait...
g++ -c -o option.o -pipe -m64 -DQMAKE_OPENSOURCE_EDITION -g -I. -Igenerators -Igenerators/unix -Igenerators/win32 -Igenerators/mac -Igenerators/symbian -Igenerators/integrity -I/home/kamal/qt-everywhere-opensource-src-4.8.2/include -I/home/kamal/qt-everywhere-opensource-src-4.8.2/include/QtCore -I/home/kamal/qt-everywhere-opensource-src-4.8.2/src/corelib/global -I/home/kamal/qt-everywhere-opensource-src-4.8.2/src/corelib/xml -I/home/kamal/qt-everywhere-opensource-src-4.8.2/tools/shared -DQT_NO_PCRE -DQT_BUILD_QMAKE -DQT_BOOTSTRAPPED -DQLIBRARYINFO_EPOCROOT -DQT_NO_TEXTCODEC -DQT_NO_UNICODETABLES -DQT_NO_COMPONENT -DQT_NO_STL -DQT_NO_COMPRESS -I/home/kamal/qt-everywhere-opensource-src-4.8.2/mkspecs/qws/linux-x86_64-g++ -DHAVE_QCONFIG_CPP -DQT_NO_THREAD -DQT_NO_QOBJECT -DQT_NO_GEOM_VARIANT -DQT_NO_DEPRECATED  option.cpp
g++ -o "/home/kamal/qt-everywhere-opensource-src-4.8.2/bin/qmake" project.o property.o main.o makefile.o unixmake2.o unixmake.o mingw_make.o option.o winmakefile.o projectgenerator.o meta.o makefiledeps.o metamakefile.o xmloutput.o pbuilder_pbx.o borland_bmake.o msvc_vcproj.o msvc_vcxproj.o msvc_nmake.o msvc_objectmodel.o msbuild_objectmodel.o symmake.o initprojectdeploy_symbian.o symmake_abld.o symmake_sbsv2.o symbiancommon.o registry.o epocroot.o gbuild.o qtextcodec.o qutfcodec.o qstring.o qtextstream.o qiodevice.o qmalloc.o qglobal.o qbytearray.o qbytearraymatcher.o qdatastream.o qbuffer.o qlist.o qfile.o qfilesystementry.o qfilesystemengine_unix.o qfilesystemengine.o qfilesystemiterator_unix.o qfsfileengine_unix.o qfsfileengine.o qfsfileengine_iterator.o qregexp.o qvector.o qbitarray.o qdir.o qdiriterator.o quuid.o qhash.o qfileinfo.o qdatetime.o qstringlist.o qabstractfileengine.o qtemporaryfile.o qmap.o qmetatype.o qsettings.o qsystemerror.o qlibraryinfo.o qvariant.o qvsnprintf.o qlocale.o qlocale_tools.o qlocale_unix.o qlinkedlist.o qurl.o qnumeric.o qcryptographichash.o qxmlstream.o qxmlutils.o  
The OpenGL ES 2.0 functionality test failed!
 You might need to modify the include and library search paths by editing
 QMAKE_INCDIR_OPENGL, QMAKE_LIBDIR_OPENGL and QMAKE_LIBS_OPENGL in
 /home/kamal/qt-everywhere-opensource-src-4.8.2/mkspecs/qws/linux-TIarmv7-sgx-g++.

=================================================================================================================================

this linux-TIarmv7-sgx-g++ : qmake.conf

#
# qmake configuration for building with arm-linux-g++
#

include(../../common/gcc-base-unix.conf)
include(../../common/g++-unix.conf)
include(../../common/linux.conf)
include(../../common/qws.conf)

#User specific Path - To Be edited by User
QT_INSTALL_DIR          = /home/kamal/qt-everywhere-opensource-src-4.8.2
SGX_SDK_ROOT            = /home/kamal/Graphics_SDK_4_09_00_01
TSLIB_INCDIR            =
TSLIB_LIBDIR            =

# modifications to g++.conf
QMAKE_CFLAGS_RELEASE    = -O3 -march=armv7-a -mtune=cortex-a8 -mfpu=neon -mfloat-abi=softfp
QMAKE_CXXFLAGS_RELEASE    = -O3 -march=armv7-a -mtune=cortex-a8 -mfpu=neon -mfloat-abi=softfp
QMAKE_CC                = arm-linux-gnueabihf-gcc
QMAKE_CXX               = arm-linux-gnueabihf-g++
QMAKE_LINK              = arm-linux-gnueabihf-g++
QMAKE_LINK_SHLIB        = arm-linux-gnueabihf-g++

# modifications to linux.conf
QMAKE_AR                = arm-linux-gnueabihf-ar cqs
QMAKE_OBJCOPY           = arm-linux-gnueabihf-objcopy
QMAKE_STRIP             = arm-linux-gnueabihf-strip

#Do not edit beyond this

QMAKE_INCDIR_OPENGL_ES2 = $$SGX_SDK_ROOT/GFX_Linux_SDK/OGLES2/SDKPackage/Builds/OGLES2/Include/
QMAKE_INCDIR_OPENGL_ES2 += $$SGX_SDK_ROOT/GFX_Linux_SDK/OGLES2/SDKPackage/Builds/OGLES2/LinuxOMAP3/Include/
QMAKE_INCDIR_OPENGL_ES2 += $$SGX_SDK_ROOT/include
QMAKE_INCDIR_OPENGL_ES2 += $$SGX_SDK_ROOT/GFX_Linux_SDK/OGLES/SDKPackage/Builds/OGLES/Include/
QMAKE_LIBDIR_OPENGL_ES2 = $$SGX_SDK_ROOT/gfx_dbg_es8.x/
QMAKE_LIBS_OPENGL_ES2   = -lEGL -lGLESv2 -lGLES_CM -lIMGegl -lsrv_um -lusc

QMAKE_INCDIR_OPENGL     += $$SGX_SDK_ROOT/GFX_Linux_SDK/OGLES/SDKPackage/Builds/OGLES/Include/
QMAKE_LIBDIR_OPENGL     = $$SGX_SDK_ROOT/gfx_dbg_es8.x
QMAKE_LIBDIR_OPENGL_QT  = $$SGX_SDK_ROOT/gfx_dbg_es8.x
QMAKE_LIBS_OPENGL_ES1   = -lEGL -lGLES_CM -lIMGegl -lsrv_um -lusc

QMAKE_INCDIR_OPENVG     = $$SGX_SDK_ROOT/GFX_Linux_SDK/OVG/SDKPackage/Builds/OVG/Include/
QMAKE_LIBDIR_OPENVG     = $$SGX_SDK_ROOT/gfx_dbg_es8.x/
QMAKE_LIBS_OPENVG       = -lEGL -lGLESv2 -lGLES_CM -lIMGegl -lsrv_um -lOpenVG -lOpenVGU

QMAKE_INCDIR_EGL        = $$QMAKE_INCDIR_OPENGL_ES2
QMAKE_INCDIR_EGL        += $$QT_INSTALL_DIR/src/3rdparty/powervr/wsegl2
QMAKE_INCDIR_POWERVR    = $$QT_INSTALL_DIR/src/3rdparty/powervr/wsegl2
QMAKE_LIBDIR_EGL        = $$QMAKE_LIBDIR_OPENGL_ES2
QMAKE_LIBS_EGL          = -lEGL -lIMGegl -lsrv_um -lGLESv2 -lGLES_CM -lusc

QMAKE_INCDIR += $$TSLIB_INCDIR
QMAKE_INCDIR += $$QMAKE_INCDIR_OPENGL_ES2
QMAKE_LIBDIR += $$QMAKE_LIBDIR_OPENGL_ES2
QMAKE_LIBDIR += $$TSLIB_LIBDIR
#QMAKE_LIBS = $$QMAKE_LIBS_OPENGL_ES2 -lts
QMAKE_LIBS = $$QMAKE_LIBS_OPENGL_ES2
load(qt_config)

==========================================================================================================================================

how can i solve this failure ?