This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLR on AM57xx

Hi is DLR supported on the AM57xx processors in the PRU. 

Is it just client mode that is supported or is Supervisor mode also supported. 

Also are there any royalty fees for using the DLR code for the PRU. 

Thanks in Advance. 

  • Hi Sunil, 

    This support will be added in the forthcoming release on AM57xx which should be towards end of Jan. Support will be for client mode and there will be no royalty for the driver software. Also please note that the PRU code is provided as a binary and sources are not public at this moment.

    Regards

    Vineet

  • Hi Vineet, 

    Thanks for the quick reply. 

    Is the code for the am337x significantly different than the am37xx for the PRU. 

    I see there is some DLR sample code in the Industrial SDK. 

    If we wanted to develop the code for the supervisor mode ourselves would that be possible. 

    Would we have access to the required libraries. 

    Thanks,

    Sunil