Can one McASP be used as TDM receiver and DIT transmitter with different sampling frequency each other?
For example:
McASP0 Receiver : TDM mode, fs=48KHz
McASP0 Transmitter: DIT mode, fs=44.1KHz
Best regards,
Daisuke
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can one McASP be used as TDM receiver and DIT transmitter with different sampling frequency each other?
For example:
McASP0 Receiver : TDM mode, fs=48KHz
McASP0 Transmitter: DIT mode, fs=44.1KHz
Best regards,
Daisuke
Hi Biser-san,
Thank you for your reply.
In section 22.1.2 of the AM335X TRM Rev. L:
" In DIT mode for McASP, additional features of the transmitter are:
- Transmit-only mode 384 time slots (subframe) per frame. "
In section 22.3.8.3.2 of the AM335X TRM Rev. L:
" The DIT transmitter only works in the following configuration:
- 384-slot TDM, XMOD = 1 1000 0000b. "
Do these not indicate that in DIT mode (DITEN=1) the transmitter works and the receiver does not work?
Best regards,
Daisuke