My system is linux-2.6.37-psp04.04.00.01-sk running on am3871, I'm using USB-Ethernet / RNDIS gadget to communicate with Windows 7/8.1 PC. It works fine with desktop or notebook PC, but not with tablet. When connecting to tablet Network adapter is created, connection works, but after 1-2 minutes the connection goes to disabled state. I need to reconnect the device to enable it back. This occurs in any case, flowing the data through the connection or not. I tested 2 different tablets and the result is the same.