This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H14 Hyperlink issue with TMS320C6678

Other Parts Discussed in Thread: TMS320C6678, 66AK2H14

Hi ,

We have a customized board with one K2H14 and three TMS320C6678. The Hyperlink are connected as per the attached diagram                              

In our customized board we have initialized the K2H14 and C6678 to 10GBPS.

We are using the hyplnk_K2HC66BiosExampleProject for the K2H14.

We are using the Hyperlink clock - 156.25MHz

And in the hyplnk_K2HC66BiosExampleProject we have customized the clock as per our board support and also we have changed the code for External Data Transfer.

K2H14 as Receiver and C6678 as Transmitter - we are receiving the Data in the K2H14 Hyperlink Data and we verified on the Hyperlink0 data (0x40000000).

 K2H14 as Transmitter and C6678 as Receiver - when K2H14 is trying to read the C6678 remote register, the K2H14 cannot able to do it.

We have also downgraded the speed and tested, but we are having the same issue.

Question:

--------------

 What can be the cause for the issue?

Regards,

Sakthi.Ahyperlink.doc