This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C674x MP3 Decoder Streaming

Hi,

I would like to develop an application to play (decode in real-time) MP3 files using a C674x DSP. This would require an MP3 decoder, which is available for C674x here:

Before I spend time trying to set this up, I want to ask if it is possible to use this decoder to stream MP3 files and not just decode an MP3 file to a PCM file. I would like to stream MP3 files, so decoding PCM samples and outputting via McASP on-the-fly. Is this possible using this example MP3 decoder?

Thanks

Brian