Hi,
I am wanting to use the RTOS Analyzer (Task Profile) with my code running on a 5517 DSP. When I click on it I get an error saying could not detect a UIA configuration. I tried to create a UIA configuration using the document "Systems Analyzer User Guilde - section 5.1 Quickly Enabling UIA Instrumentation" at http://www.ti.com/lit/ug/spruh43f/spruh43f.pdf,
I attempted the directions in 5.1. Using XGCONF to Enable UIA Instrumentation but no matter what I try I get "org.eclipse.rtsc.xdctools.INVALID_RTSC_TARGET: Invalid target"
The only RTSC option I can find to enable is in <properties> <C/C++ general> <Configure Workspace Properties> and there I cannot determine what Target: or Platform to select.
Can You help me?
Regards,
Steve