I'm using EVMK2E, the DSP is C66AK2E05. No matter I configure the IP address manully or danymically, I can't ping the dsp successfully.
when mannuly, work the console shows that network added, however , but I can't ping it successfully. It comes to be "Destination host Unreachable".
When dynamically, the console shows that the DHCP running. I can't get the IP. I use the "arp -a" command ,but no information. how can I do to run the priject right?
When I use Static IP, I set the PC IP manully such as 192.168.0.100, and I will set the LocalIPaddr as well as the DSP IP 192.168.0.102, the are in the same subnet. But I can't Ping it sucessfully. With the "arp -a", I can't find the DSP MAC. I don't know why. Really need you help. Thank you. Looking forward you reply.