This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ARM and DSP UART testing in EVMK2E

We are working on a reference EVMK2E board.

There is two uart in the board

1.ARM UART - UART 1

2.BMC UART - UART 2

I need to test and verify transmit and receive operation of both UART.

I have a simple linux UART Transmit and Receive Application which I can use in ARM to verify UART1 operation

and for UART 1, I verified it through that UART transmit and receive application.

And for UART2, how can I verify the transmit and receive operation ??

Whether its possible to use that kind of application in UART2 to verify the Transmit and Receive operation or through some other application ?

Please clarify me on this.

Thanks & Regards,

Sarjoon.