Dear sir,
I want to work on c6713 with CCS5.3 and MATLAB2011A.Can i get the documents related to the procedure of it.
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear sir,
I want to work on c6713 with CCS5.3 and MATLAB2011A.Can i get the documents related to the procedure of it.
thank you
Hi Mohammad,
please refer to the following TI WIKI.

Hi,
MATLAB2011a is not compatible to CCSv5 and it is not supported. Kindly check the below mathworks links:
http://www.mathworks.com/matlabcentral/answers/58500-is-ccsv5-compatible-to-matlab2011a
http://www.mathworks.com/matlabcentral/answers/41444-ti-ccsv5-support-for-ide-link
To know more answers on the CCSvx.0 compatibility with MATLAB, you could get it from the below matlab central:
http://www.mathworks.com/matlabcentral/answers/?term=MATLAB2011A
Please search the keyword to get answers appropriately from search window on the above MATLAB central answers Mathworks forum.
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question
-------------------------------------------------------------------------------------------------------
Hi Mohammad,
I could see the same question as a duplicate post here too.

I would request you to follow up with any one of the threads and close this one