This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Test NAND flash through an example project on evmk2h?

Hi,

We developed a custom board that is exactly same as EVMK2H. Now we are in phase of board testing. We want to test all the interfaces i.e PCIe, SRIO, Hyperlink, UART, NOR and NAND flash. We came across example projects for most of interfaces except NAND,NOR and USB. We are not able to use u-boot as we encountered some issues in DDR3 and U-boot halts/stuck at DDR3. How can we test interfaces in our situation? 

We also ran platform test it indicated NOR test Passed and NAND failed with error -19. What does that mean? Remember our NAND flash is unpartitioned( no partitions are created).

Regards