This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DMAQNUM register of EDMA accessed simultaneously by ARM and DSP (DM6467)

DM6467 hardware architecture supports both ARM and DSP accessing the EDMA resources. Simultaneous access by both ARM and DSP to the EDMA registers is not protected in software architecture. Since simultaneous access to EDMA HW registers by DSP and ARM is not protected, it can expose a bug which can cause a deadlock situation . As per this silicon errata, if L2 and DDR/HDVICP writes are submitted on same TC, there could be a system deadlock. To avoid this situation of deadlock, L2 writes should never be submitted on TC sharing DDR/HDVICP writes.


To avoid GEM lockup situation we could dedicate one TC for L2 writes. TC0, TC1 and TC3 are used for DDR and HDVICP writes. The TC used by a particular EDMA channel is controlled by setting DMAQNUMn register. IF  both CPUs perform read->modify->write operation on this register, it can happen that one of these processors is reading the register value while it is in the update cycle by other CPU. If EDMA channel corresponding to L2 writes by DSP shares the DMAQNUMn register used by ARM, following series of event as illustrated in the figure below can accidentally push L2 and DDR writes to same TC causing the deadlock bug to show up.

To avoid such a case, care should be taken in the system such that the ARM and the DSP do not access these registers simultaneoulsy.