Hi,
My customer has the following questions regarding TMS320C6455 DDR capacity and type:
1. The C6455 DSP states that the DDR2 interface has a limitation of 512 MB of address space. Do you know if this space can be "paged"? In other words, are we able to hang more than 512 MB off of this bus and effectively be able to read/write to it? 512 MB seems like a fairly small amount considering the size of available DDR2 memory devices.
2. Can a DDR2 DIMM be used with this device? It would seem unusual to have a DDR2 interface without the capability of supporting the large selection of DIMMs in the industry.
Thanks,
Rick