Hello,
We have an application where we need to either disable unused OMAP-L138 peripherals, or else somehow explain that they won't interfere with normal operation.
I have figured out how to disable most of the unused peripherals, but I can't find any way to individually disable the peripherals below without also disabling some peripherals we need. I thought about trying to disable them by disabling the specific clocks that they use, but after looking at SRUH77A table 8-1, I see this would also disable perihperals we need. Any ideas how we can individually disable the peripherals below? (or explain in a credible way that they are gauranteed to not intefere with our application?)
ETM_ETB |
Embedded Trace Macrocell / Embedded Trace Buffer |
McASP |
Multichannel Audio Serial Port |
McBSP |
Multichannel Audio Serial Port |
I2C |
Inter-Integrated Circuit Serial Ports |
LCDC |
LCD Controller |
VPIF |
Video Port Interface |
eHRPWM |
Enhanced High-Resolution Pulse-Width Modulator (eHRPWM) |
eCAP |
Enhanced Capture Peripheral |
USB1_1_OHCI |
Universal Serial Bus Host Controller |
EMAC |
Ethernet Media Access Controller |