Please tell me the input impedance of the USBx_VBUS.
The USBx_DRVVBUS does not use to control an external 5V charge pump because the 5V VBUS power is always supplied after the system is powered-up. The USBx_VBUS may be connected to a 5V digital output to be controlled by an external device, e.g. USB HUB IC, but it is analog input. To connect a 5V digital output to the USBx_VBUS, I want to know the input impedance of the USBx_VBUS.
Best regards,
Daisuke