This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

156 Lines Limit of AEW engine in vertical direction



Dear All:

 

When we want to set our AEW windows into the center of the frame,

we find there is a checking rule in the driver, dm355_aew.c which will limit

the max vertical measure distance to 156 lines.

But I seem not to be able to find this limit in the datasheet, even not from

the more detailed data of VPFE coming from domestic TI FAE, after we sign NDA.

Can any one explain this rule for me or is there any way to put the AEW windows

in the center of the frame (especially in the vertical direction)?

Thank you in advance.

 

Best regards,

 

Ray