My customer is using a AM335x with DDR3 memory (16bit-width).
#All DATA0_REG_XXXX and DAta1_REG_XXXX are the same value.
Best Regards,
Takahiro Ogo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Taka-san
Can you share a little more information on the tDQSS measurements that you've? Are you running JEDEC compliance tests?
Some possible reasons for the differences in the DQS0 vs. DQS1 delay could be the following:
1) Are the layers on which the traces are routed the same? If so, do they have similar Td profile? Do they have equal VIA's? The best way to validate all of this is to run a simulation extracting the board layout
2) Load capacitance on the memory input could have been different between DQS0 and DQS1 - I don't have the memory part/IBIS model to confirm this, but this is a likely possibility
Regards, Siva
Hi Siva-san
Thank you for your kind supoort. Please excuse me for the delay.
sivak said:
Can you share a little more information on the tDQSS measurements that you've? Are you running JEDEC compliance tests?
They don't do JEDEC Compliance tests. But they are runining a memory timing tests with the memory manufacturer.
As the result:
tDQSS for DQSL(DQS0) is failed.
tDQSS for DQSU(DQS1) is passed.
They are wondering that there is a difference in DQS0 and DQS1 timing in spite of the fact that DATA0_xxx and DATA1_x are set the same value.
sivak said:
1) Are the layers on which the traces are routed the same? If so, do they have similar Td profile? Do they have equal VIA's? The best way to validate all of this is to run a simulation extracting the board layout
sivak said:2) Load capacitance on the memory input could have been different between DQS0 and DQS1 - I don't have the memory part/IBIS model to confirm this, but this is a likely possibility
Thanks. I will check the memory side.
#They are using a NT5CC128M16IP-DI.
I would appreciate it very much if you could point out anything to me.
Best Regards,
Taka