Hi,
Does AM335x support booting from following nand flash?
TOSHIBA: TC58NYG2S0HBAI4
toshiba.semicon-storage.com/.../docget.jsp
The Device ID is 0xAC.
This Device ID is listed in Table 26-14 Supported NAND Devices of TRM.
This NAND flash is comprised of the following.
(4096 + spare 256) *64 bytes pages X 2048blocks
There are following mentions in 26.1.7.4.1 Features of TRM.
Support for large page size (2048 +64 4096 +128 bytes spare bytes) or very large page size bytes /)
218 spare bytes)
The spare size of this NAND is 256 byte, is there a problem?
Best Regards,
Shigehiro Tsuda