Other Parts Discussed in Thread: AM5728, DRA752, PMP, BEAGLEBOARD-X15, TLC59108, TMP102, TLV320AIC3104, ASH
Dear All,
I am working with processor SDK with Customized board designed with AM5728. While booting it is getting crashed with the following. Can any one help on this. we are working on this kind of issues since long time.
U-Boot SPL 2015.07-dirty (Dec 07 2015 - 08:20:44)
DRA752 ES1.1
reading args
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
U-Boot 2015.07-dirty (Dec 07 2015 - 08:20:44 +0530)
CPU : DRA752 ES1.1
Board: BeagleBoard x15
I2C: ready
DRAM: 512 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net: Phy 1 not found
cpsw
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
604 bytes read in 4 ms (147.5 KiB/s)
Loaded environment from uEnv.txt
Importing environment from mmc0 ...
3326720 bytes read in 176 ms (18 MiB/s)
87672 bytes read in 25 ms (3.3 MiB/s)
Booting from mmc0 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x32c300 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe7000, end 8ffff677 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.1.6-g52c4aa7 (medha@medha) (gcc version 4.9.3 20150413 (prerelease) (Linaro GCC 4.9-2015.05) ) #3 PREEMP6
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI AM5728 BeagleBoard-X15
[ 0.000000] cma: Reserved 24 MiB at 0x9e400000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] DRA752 ES1.1
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129408
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=00000000-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 482756K/522240K available (6315K kernel code, 319K rwdata, 2216K rodata, 272K init, 231K bss, 14908K reserved, 2)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc085d05c (8533 kB)
[ 0.000000] .init : 0xc085e000 - 0xc08a2000 ( 272 kB)
[ 0.000000] .data : 0xc08a2000 - 0xc08f1f68 ( 320 kB)
[ 0.000000] .bss : 0xc08f4000 - 0xc092dcb8 ( 232 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Additional per-CPU info printed with stalls.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] OMAP clockevent source: timer1 at 32768 Hz
[ 0.000000] clocksource 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 65535999984741ns
[ 0.000030] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000366] Architected cp15 timer(s) running at 6.14MHz (virt).
[ 0.000396] clocksource arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000401] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000409] Switching to timer-based delay loop, resolution 162ns
[ 0.000888] Console: colour dummy device 80x30
[ 0.000902] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000906] This ensures that you still see kernel messages. Please
[ 0.000910] update your kernel commandline.
[ 0.000917] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000927] pid_max: default: 32768 minimum: 301
[ 0.000979] Security Framework initialized
[ 0.001005] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.001012] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.001415] Initializing cgroup subsys blkio
[ 0.001426] Initializing cgroup subsys memory
[ 0.001447] Initializing cgroup subsys devices
[ 0.001457] Initializing cgroup subsys freezer
[ 0.001465] Initializing cgroup subsys perf_event
[ 0.001481] CPU: Testing write buffer coherency: ok
[ 0.001641] Setting up static identity map for 0x80008200 - 0x80008258
[ 0.002561] devtmpfs: initialized
[ 0.020391] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.020845] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.027778] omap_hwmod: tptc0 using broken dt data from edma-controller
[ 0.028015] omap_hwmod: tptc1 using broken dt data from edma-controller
[ 0.164483] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.165126] pinctrl core: initialized pinctrl subsystem
[ 0.165718] NET: Registered protocol family 16
[ 0.166410] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.171621] OMAP GPIO hardware version 0.1
[ 0.187616] No ATAGs?
[ 0.187635] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.187642] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.189858] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.189865] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.190128] OMAP DMA hardware revision 0.0
[ 0.226118] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[ 0.228141] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver
[ 0.230610] vgaarb: loaded
[ 0.230918] SCSI subsystem initialized
[ 0.231104] usbcore: registered new interface driver usbfs
[ 0.231148] usbcore: registered new interface driver hub
[ 0.231197] usbcore: registered new device driver usb
[ 0.232041] palmas 0-0058: IRQ missing: skipping irq request
[ 0.250692] palmas 0-0058: Muxing GPIO 2e, PWM 0, LED 0
[ 0.312527] pcf857x 0-0020: probed
[ 0.313016] pcf857x 0-0021: probed
[ 0.313113] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.313248] pps_core: LinuxPPS API ver. 1 registered
[ 0.313254] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.313277] PTP clock support registered
[ 0.313571] Advanced Linux Sound Architecture Driver Initialized.
[ 0.314034] Switched to clocksource arch_sys_counter
[ 0.320508] NET: Registered protocol family 2
[ 0.320963] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.320997] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.321050] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.321087] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.321102] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.321188] NET: Registered protocol family 1
[ 0.321353] RPC: Registered named UNIX socket transport module.
[ 0.321359] RPC: Registered udp transport module.
[ 0.321364] RPC: Registered tcp transport module.
[ 0.321368] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.322102] CPU PMU: Failed to parse /pmu/interrupt-affinity[0]
[ 0.322140] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.323443] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.323495] audit: initializing netlink subsys (disabled)
[ 0.323521] audit: type=2000 audit(0.310:1): initialized
[ 0.327986] VFS: Disk quotas dquot_6.6.0
[ 0.328097] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.329390] NFS: Registering the id_resolver key type
[ 0.329413] Key type id_resolver registered
[ 0.329418] Key type id_legacy registered
[ 0.329466] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 0.331324] alg: No test for stdrng (krng)
[ 0.331351] NET: Registered protocol family 38
[ 0.331392] io scheduler noop registered
[ 0.331403] io scheduler deadline registered
[ 0.331432] io scheduler cfq registered (default)
[ 0.333970] pinctrl-single 4a003400.pinmux: 281 pins at pa fc003400 size 1124
[ 0.362140] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[ 0.362151] pci_bus 0000:00: root bus resource [io 0x1000-0xffff]
[ 0.362159] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 0.362168] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 0.362463] PCI: bus0: Fast back to back transfers disabled
[ 0.362557] PCI: bus1: Fast back to back transfers enabled
[ 0.362630] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 0.362642] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 0.362651] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 0.363970] OMAP DSS rev 6.1
[ 0.364218] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[ 0.380351] tlc59108 0-0040: Successfully initialized tlc59108
[ 0.420029] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.422325] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 299, base_baud = 3000000) is a 8250
[ 1.196203] console [ttyS0] enabled
[ 1.200469] [drm] Initialized drm 1.1.0 20060810
[ 1.211141] brd: module loaded
[ 1.217268] loop: module loaded
[ 1.221018] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.228938] usbcore: registered new interface driver smsc95xx
[ 1.234966] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.241524] ehci-pci: EHCI PCI platform driver
[ 1.246036] ehci-omap: OMAP-EHCI Host Controller driver
[ 1.251584] mousedev: PS/2 mouse device common for all mice
[ 1.257243] i2c /dev entries driver
[ 1.261663] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 1.266525] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr104 mode
[ 1.272992] omap_hsmmc 4809c000.mmc: no pinctrl state for hs200_1_8v mode
[ 1.279833] omap_hsmmc 4809c000.mmc: no pinctrl state for ddr50 mode
[ 1.286223] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr50 mode
[ 1.292600] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr25 mode
[ 1.298987] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr12 mode
[ 1.305374] omap_hsmmc 4809c000.mmc: no pinctrl state for hs mode
[ 1.311490] omap_hsmmc 4809c000.mmc: no pinctrl state for ddr_1_8v mode
[ 1.344268] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.351465] oprofile: using timer interrupt.
[ 1.355976] Initializing XFRM netlink socket
[ 1.360281] NET: Registered protocol family 17
[ 1.364788] NET: Registered protocol family 15
[ 1.369306] Key type dns_resolver registered
[ 1.373678] omap_voltage_late_init: Voltage driver support not added
[ 1.380236] Power Management for TI OMAP4+ devices.
[ 1.385316] ThumbEE CPU extension supported.
[ 1.389610] Registering SWP/SWPB emulation handler
[ 1.395493] dmm 4e000000.dmm: workaround for errata i878 in use
[ 1.402755] dmm 4e000000.dmm: initialized all PAT entries
[ 1.425941] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.432583] [drm] No driver support for vblank timestamp query.
[ 1.438570]
Connector Detailsdisplay0: 1 (force=1)
[ 1.467645] [drm] Enabling DMM ywrap scrolling
[ 1.548360] Console: switching to colour frame buffer device 160x50
[ 1.562016] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
[ 1.567969] omapdrm omapdrm.0: registered panic notifier
[ 1.594059] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0
[ 1.600897] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 1.605754] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr104 mode
[ 1.612221] omap_hsmmc 4809c000.mmc: no pinctrl state for hs200_1_8v mode
[ 1.619047] omap_hsmmc 4809c000.mmc: no pinctrl state for ddr50 mode
[ 1.625434] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr50 mode
[ 1.631812] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr25 mode
[ 1.638199] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr12 mode
[ 1.644586] omap_hsmmc 4809c000.mmc: no pinctrl state for hs mode
[ 1.650704] omap_hsmmc 4809c000.mmc: no pinctrl state for ddr_1_8v mode
[ 1.744051] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[ 1.750173] davinci_mdio 48485000.mdio: detected phy mask fffffff3
[ 1.760351] libphy: 48485000.mdio: probed
[ 1.764410] davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver unknown
[ 1.772447] davinci_mdio 48485000.mdio: phy[3]: device 48485000.mdio:03, driver unknown
[ 1.780884] cpsw 48484000.ethernet: Detected MACID = 74:da:ea:0c:dc:a2
[ 1.788061] cpsw 48484000.ethernet: cpsw: Detected MACID = 74:da:ea:0c:dc:a3
[ 1.795585] hctosys: unable to open rtc device (rtc0)
[ 1.807000] vdd_3v3: disabling
[ 1.810094] mmc0: host does not support reading read-only switch, assuming write-enable
[ 1.818288] ALSA device list:
[ 1.821263] No soundcards found.
[ 1.824746] mmc0: new SDHC card at address aaaa
[ 1.829800] mmcblk0: mmc0:aaaa SS08G 7.40 GiB
[ 1.835591] mmcblk0: p1 p2
[ 1.854783] EXT4-fs (mmcblk0p2): warning: mounting fs with errors, running e2fsck is recommended
[ 1.870405] EXT4-fs (mmcblk0p2): recovery complete
[ 1.875247] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 1.883388] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 1.892778] devtmpfs: mounted
[ 1.895927] Freeing unused kernel memory: 272K (c085e000 - c08a2000)
INIT: version 2.88 booting
Starting udev
[ 2.690708] udevd[69]: starting version 182
[ 2.978208] Unable to handle kernel NULL pointer dereference at virtual address 00000030
[ 2.986340] pgd = dc9a0000
[ 2.989053] [00000030] *pgd=9c982831, *pte=00000000, *ppte=00000000
[ 2.995365] Internal error: Oops: 817 [#1] PREEMPT ARM
[ 3.000521] Modules linked in:
[ 3.003592] CPU: 0 PID: 88 Comm: udevd Not tainted 4.1.6-g52c4aa7 #3
[ 3.009969] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 3.016085] task: dc8ef600 ti: dc99a000 task.ti: dc99a000
[ 3.021512] PC is at account_page_dirtied+0x160/0x1d8
[ 3.026585] LR is at contig_page_data+0x0/0xac0
[ 3.031131] pc : [<c00c78b0>] lr : [<c08eff98>] psr: 60000093
[ 3.031131] sp : dc99be40 ip : 0000000e fp : dc99be7c
[ 3.042655] r10: 0009c9ba r9 : 00000000 r8 : 00000000
[ 3.047899] r7 : 00000000 r6 : c08eff98 r5 : 00000000 r4 : de385e28
[ 3.054450] r3 : c08b89c0 r2 : 00020171 r1 : 00000015 r0 : 000002c8
[ 3.061002] Flags: nZCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment user
[ 3.068251] Control: 10c5387d Table: 9c9a0059 DAC: 00000015
[ 3.074018] Process udevd (pid: 88, stack limit = 0xdc99a210)
[ 3.079784] Stack: (0xdc99be40 to 0xdc99c000)
[ 3.084158] be40: c090cab4 00200200 c08eff98 20000013 dc8cca50 00000000 dc985e18 b6ff8000
[ 3.092369] be60: dc99bee0 dc8cca50 dc985dc0 b6ff7000 dc99be94 dc99be80 c00c4290 c00c4070
[ 3.100579] be80: 00000000 dc985e18 dc99bea4 dc99be98 c00c4458 c00c4254 dc99beb4 dc99bea8
[ 3.108788] bea0: c00c4474 c00c4434 dc99bf2c dc99beb8 c00e754c c00c4468 dc90ec40 00000000
[ 3.116997] bec0: dc8cca50 b6ff7000 b6ff8000 bf000000 00000000 00000000 00000400 dc9ba000
[ 3.125207] bee0: c08f4cd8 00001000 dc99bf2c dc99bef8 c00e78dc c00e6f84 c00e8414 c00e7cc4
[ 3.133416] bf00: dc8cca50 dc90ec40 dc8cca50 00000000 b6ff7000 dc90ec44 dc985dc0 dc8cca50
[ 3.141625] bf20: dc99bf6c dc99bf30 c00e937c c00e7408 b6ff8000 ffffffff 00000000 dc985dc8
[ 3.149834] bf40: 00000000 dc90ec74 dc90ec40 b6ff7000 00001000 c000f9c4 dc99a000 00000000
[ 3.158044] bf60: dc99bf8c dc99bf70 c00e957c c00e9154 b6ff7000 00001000 00000000 0000005b
[ 3.166252] bf80: dc99bfa4 dc99bf90 c00ea514 c00e9544 00044308 00000000 00000000 dc99bfa8
[ 3.174461] bfa0: c000f820 c00ea4fc 00044308 00000000 b6ff7000 00001000 00000000 b6ff8000
[ 3.182670] bfc0: 00044308 00000000 00000000 0000005b 00000000 00043488 00043488 0006d680
[ 3.190879] bfe0: 00000006 be9dcfc4 b6eb708d b6ef9de6 20000030 b6ff7000 00000000 00000000
[ 3.199084] Backtrace:
[ 3.201549] [<c00c4064>] (free_hot_cold_page) from [<c00c4290>] (__free_pages+0x48/0x4c)
[ 3.209670] r10:b6ff7000 r9:dc985dc0 r8:dc8cca50 r7:dc99bee0 r6:b6ff8000 r5:dc985e18
[ 3.217561] r4:00000000
[ 3.220110] [<c00c4248>] (__free_pages) from [<c00c4458>] (free_pages.part.90+0x30/0x34)
[ 3.228230] r5:dc985e18 r4:00000000
[ 3.231833] [<c00c4428>] (free_pages.part.90) from [<c00c4474>] (free_pages+0x18/0x1c)
[ 3.239786] [<c00c445c>] (free_pages) from [<c00e754c>] (unmap_region+0x150/0x180)
[ 3.247388] [<c00e73fc>] (unmap_region) from [<c00e937c>] (do_munmap+0x234/0x3f0)
[ 3.254897] r10:dc8cca50 r9:dc985dc0 r8:dc90ec44 r7:b6ff7000 r6:00000000 r5:dc8cca50
[ 3.262784] r4:dc90ec40
[ 3.265334] [<c00e9148>] (do_munmap) from [<c00e957c>] (vm_munmap+0x44/0x58)
[ 3.272405] r10:00000000 r9:dc99a000 r8:c000f9c4 r7:00001000 r6:b6ff7000 r5:dc90ec40
[ 3.280295] r4:dc90ec74
[ 3.282843] [<c00e9538>] (vm_munmap) from [<c00ea514>] (SyS_munmap+0x24/0x28)
[ 3.290003] r7:0000005b r6:00000000 r5:00001000 r4:b6ff7000
[ 3.295715] [<c00ea4f0>] (SyS_munmap) from [<c000f820>] (ret_fast_syscall+0x0/0x3c)
[ 3.303398] r5:00000000 r4:00044308
[ 3.306999] Code: e5832004 e1c523d0 e2922001 e2a33000 (e1c523f0)
[ 3.313117] ---[ end trace edc2632e2041dcdb ]---
[ 3.495859] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
[ 3.611317] rtc rtc0: 48838000.rtc: dev (254:0)
[ 3.662579] omap_rtc 48838000.rtc: rtc core: registered 48838000.rtc as rtc0
udevd[69]: worker [153] terminated by signal 11 (Segmentation fault)
udevd[69]: worker [153] failed while handling '/devices/platform/44000000.ocp/4a080000.ocp2scp/4a084400.phy'
[ 4.205887] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 4.213771] libata version 3.00 loaded.
[ 4.233397] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
[ 4.273703] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
[ 4.337407] ahci 4a140000.sata: SSS flag set, parallel bus scan disabled
[ 4.532755] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
[ 4.574102] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[ 4.582672] ahci 4a140000.sata: flags: 64bit ncq sntf stag pm led clo only pmp pio slum part ccc apst
[ 4.762468] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
[ 4.888138] extcon-usb-gpio extcon_usb1: GPIO lookup for consumer id
[ 4.916267] extcon-usb-gpio extcon_usb1: using device tree for GPIO lookup
[ 4.941600] scsi host0: ahci
[ 4.994057] Unable to handle kernel paging request at virtual address 00087010
[ 5.001313] pgd = dba10000
[ 5.004024] [00087010] *pgd=9b9f2831, *pte=00000000, *ppte=00000000
[ 5.010339] Internal error: Oops: 80000007 [#2] PREEMPT ARM
[ 5.015928] Modules linked in: ahci_platform(+) libahci_platform libahci extcon_usb_gpio(+) cpufreq_voltdm omap_wdt libata phy_omap_e
[ 5.035034] CPU: 0 PID: 201 Comm: udevd Tainted: G D 4.1.6-g52c4aa7 #3
[ 5.042716] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 5.048829] task: db97ba80 ti: dba0a000 task.ti: dba0a000
[ 5.054245] PC is at 0x87010
[ 5.057131] LR is at 0x6000000
[ 5.060193] pc : [<00087010>] lr : [<06000000>] psr: 00000013
[ 5.060193] sp : dba0bd88 ip : 01e51600 fp : dba0bda4
[ 5.071713] r10: dba12db0 r9 : 0008fc4e r8 : db9a4c40
[ 5.076953] r7 : b6d98000 r6 : db9f1420 r5 : da8ea000 r4 : 00008816
[ 5.083501] r3 : 00000088 r2 : 00000004 r1 : cfc4ed80 r0 : 0004f2b0
[ 5.090050] Flags: nzcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
[ 5.097210] Control: 10c5387d Table: 9ba10059 DAC: 00000015
[ 5.102973] Process udevd (pid: 201, stack limit = 0xdba0a210)
[ 5.108825] Stack: (0xdba0bd88 to 0xdba0c000)
[ 5.113195] bd80: cfc4e000 c001e2ac de1b7af8 de33c0e8 dba0bde4 dba0bda8
[ 5.121402] bda0: c00e197c c001e288 00000000 00000000 dba0bdd4 de1b7af8 00000000 de1b7af8
[ 5.129609] bdc0: db9f1420 8fc4e3cf b6d98000 db9a4c40 db9f3660 db9a4c40 dba0be34 dba0bde8
[ 5.137816] bde0: c00e3228 c00e18f4 8fc4e3cf de1b7af8 db9f1318 b6d81000 00000001 b6d98000
[ 5.146023] be00: dba0be34 dba0be10 0000000a db9a4c40 c08b89c0 00000001 b6d98000 8fc4e3cf
[ 5.154230] be20: c08a4284 db9f1420 dba0beac dba0be38 c00e502c c00e316c dba12db0 8fc4e3cf
[ 5.162436] be40: dba0be8c dba0be50 c00c40fc c00c3b50 00000660 00000198 00000040 dba12db0
[ 5.170642] be60: dd878c00 00000054 00000000 b6d81000 dba0bef0 dca60630 00000006 db9f3604
[ 5.178849] be80: db9a4c40 dba0bfb0 0000081f db9a4c40 b6d98010 db97ba80 db9a4c74 00000055
[ 5.187055] bea0: dba0befc dba0beb0 c062fc20 c00e4648 c00c4474 c00c4434 dba0bf3c dba0bec8
[ 5.195262] bec0: c00e754c 00000000 00000800 00000000 dca60630 c08a85a4 0000081f c062f918
[ 5.203467] bee0: b6d98010 dba0bfb0 00000001 b6ff8be8 dba0bfac dba0bf00 c0009298 c062f924
[ 5.211673] bf00: dca60630 00000000 00000015 0007e000 db9a4c44 db9f1160 dba0bf3c dba0bf28
[ 5.219880] bf20: c00e73f4 c00fb478 db9a4c40 dca60630 dba0bf7c dba0bf40 c00e9398 c00e73ac
[ 5.228086] bf40: 00093000 c000f9c4 dba0a000 db9f1168 dba0bf6c 0007e000 db9a4c40 00093000
[ 5.236292] bf60: db9a4c74 0007e000 dba0a000 00000000 dba0bfa4 dba0bf80 c00e9a0c c0061614
[ 5.244498] bf80: 00093000 fffeb000 b6f54bd0 b6fdcb30 800d0030 ffffffff 10c5387d 10c5387d
[ 5.252704] bfa0: 00000000 dba0bfb0 c062f580 c0009264 b6e66000 b6e70ef4 00000000 b6e8e949
[ 5.260911] bfc0: b6d81000 00017010 b6fef220 b6fef6e0 00000000 00000001 b6ff8be8 b6ff9d90
[ 5.269117] bfe0: ffffffff be9dcf00 b6fd8939 b6fdcb30 800d0030 ffffffff 00006369 00000000
[ 5.277320] Backtrace:
[ 5.279787] [<c001e27c>] (v6_copy_user_highpage_nonaliasing) from [<c00e197c>] (wp_page_copy.isra.95+0x94/0x3d0)
[ 5.289998] r5:de33c0e8 r4:de1b7af8
[ 5.293594] [<c00e18e8>] (wp_page_copy.isra.95) from [<c00e3228>] (do_wp_page.isra.98+0xc8/0x6a0)
[ 5.302496] r10:db9a4c40 r9:db9f3660 r8:db9a4c40 r7:b6d98000 r6:8fc4e3cf r5:db9f1420
[ 5.310374] r4:de1b7af8
[ 5.312919] [<c00e3160>] (do_wp_page.isra.98) from [<c00e502c>] (handle_mm_fault+0x9f0/0x1040)
[ 5.321559] r9:db9f1420 r8:c08a4284 r7:8fc4e3cf r6:b6d98000 r5:00000001 r4:c08b89c0
[ 5.329357] [<c00e463c>] (handle_mm_fault) from [<c062fc20>] (do_page_fault+0x308/0x3d8)
[ 5.337473] r10:00000055 r9:db9a4c74 r8:db97ba80 r7:b6d98010 r6:db9a4c40 r5:0000081f
[ 5.345354] r4:dba0bfb0
[ 5.347897] [<c062f918>] (do_page_fault) from [<c0009298>] (do_DataAbort+0x40/0xc0)
[ 5.355579] r10:b6ff8be8 r9:00000001 r8:dba0bfb0 r7:b6d98010 r6:c062f918 r5:0000081f
[ 5.363459] r4:c08a85a4
[ 5.366005] [<c0009258>] (do_DataAbort) from [<c062f580>] (__dabt_usr+0x40/0x60)
[ 5.373424] Exception stack(0xdba0bfb0 to 0xdba0bff8)
[ 5.378490] bfa0: b6e66000 b6e70ef4 00000000 b6e8e949
[ 5.386697] bfc0: b6d81000 00017010 b6fef220 b6fef6e0 00000000 00000001 b6ff8be8 b6ff9d90
[ 5.394903] bfe0: ffffffff be9dcf00 b6fd8939 b6fdcb30 800d0030 ffffffff
[ 5.401537] r8:10c5387d r7:10c5387d r6:ffffffff r5:800d0030 r4:b6fdcb30
[ 5.408286] Code: bad PC value
[ 5.411369] ---[ end trace edc2632e2041dcdc ]---
[ 5.416009] note: udevd[201] exited with preempt_count 2
[ 5.427774] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 331
[ 5.436639] of_get_named_gpiod_flags: parsed 'id-gpios' property of node '/extcon_usb1[0]' - status (0)
[ 5.446795] no flags found for id
[ 5.450195] gpio-481 (id): gpiod_set_debounce: missing set() or set_debounce() operations
[ 5.604209] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 5.794058] ata1: SATA link down (SStatus 0 SControl 300)
[ 11.604053]
Thanks & Regards,
N.V.Subbaiah.