I am using RMII interface of AM335X with TLK110.
I want to know if TLK110 device will work with Am335X RMII interface. Please let me know recommende phy whihc will work with AM335X device if TLK110 is not ok.
AM335X reference clock is given from same oscillator(50MHz) which is providing clock to TLK110 device. Is this connection is correct?.
Is RX_DV connection from PHY is required to be connected to AM335X. If yes then whihc pin i should connect it.
Regards
Manoj A