Would like to flash the image to NOR flash so on reset the ROM boot see's the bootloader i've also built and runs the bootloader which in turn discovers the profibus_slave image also on NOR flash and loads it to RAM and runs it. I've built the NOR flash bootloader as illustrated in the documentation, but I've been unable to flash it along w/the profibus_slave image to NOR flash. Can somebody point me to the correct docs?