Hello
I'm not sure if this is a question for the Ti community or beaglebone forum but my question is:
1) How would I go around using a 800x480 24bit SDR(RGB888) display with a frame rate of 120Hz for the BBB.
I'm basically using a near eye display module which is like the one used on Google Glass, the display module does not require VSYNC or HSYNC.
The BBB is currently using Debian 7.8 release 01/03/2015.
Thank you for your time.
Ben W