This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 works with TVP7002 but doesn't with ADV7611

Hello, all.

We have 2 almost identical boards with DM8148: one with TVP-7002 (analog input) connected to the Port0 16 bit, another with the ADV-7611 (DVI input) connected to the same port in the same manner exactly.

We also have the McFW based application, which works fine with TVP-7002, which produces the BT-1120 protocol with embedded sync.
But when we run it on the board with ADV-7611, the capture does not receive even a single frame.

We checked everything coming to the head - ADV emits BT-1120 clocks, we see that bits 14-15 of the BT-1120 sometimes go high, which we believe to be the embedded syncs.

The questions is: what can be checked else to locate the problem? Are there any indicators in some CPU registers, which may indicate/localize the problem? Some DMA byte counters, error registers, etc.

Many many thanks ahead for any help.