All,
This is a helpful site to help you with Hardware Schematic Review for your designs using the DM36x family of devices.
http://processors.wiki.ti.com/index.php/DM36x_Schematic_Review_Checklist
regards,
miguel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
All,
This is a helpful site to help you with Hardware Schematic Review for your designs using the DM36x family of devices.
http://processors.wiki.ti.com/index.php/DM36x_Schematic_Review_Checklist
regards,
miguel
Ulrich,
it works well for me.
http://processors.wiki.ti.com/index.php/DM36x_Schematic_Review_Checklist
You can also find it, by going to the main processors wiki http://processors.wiki.ti.com/index.php/Category:DM365 and search for it there.
Please let me know if you are able to see it now.
regards,
miguel
Hi Miguel,
now it is working fine. Perhaps it was temporarily offline. Thanks!
Regards
Ulrich
HI Miguel,
A question to you:
1. When the TMS320DM355 is in deep sleep mode, will the IO's remain in previous state or in Tri-state ?
Thanks
Regards
sudarshan
Thanks Miguel,
Couple of questions :
1. If ASPn is not used, can I leave it open ?
2. un-used SPI interface can be left open ?
Thanks
Regards
Sudarshan
Sudarshan,
1. If the ASP pins are inputs at reset, No, either program them as GPIO if muxed w/GPIO and set them as outputs to avoid them from floating, if NO GPIO capability exists then pull them up/down w/external resistors.
2. see #1.
I've put together the below guidelines for DM355, please take a look this should help you, please let us know if further questions.
regards,
miguel
Miguel,
Can TMS320dm355 support MT46H32M16LFBF-6 mDDR part. Is this been used and working fine ?
Thanks in advance.
Regards
Sudarshan
Sudarshan,
We are getting off on a completely different subject from this post announcement.
Can you please re-post in a new post? and I'll reply there.
regards,
miguel