Other Parts Discussed in Thread: TVP5158
Hello
Recently, I update GLSDK to latest. I checked that kernel version also updated to 3.14.57 in latest GLSDK.
But there are some strange message in kernel log.
Could you explain below log messages if it is ok or not?
If it can generate latent problem, please check and tell me.
Im using VAYU evm board(XC5777X CPU board) with prebuilt binary(kernel, rootfs both)
-------------------------------------------------------------------------------------------------------------------------
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 3.14.57 (tiiappadmin@swubn01) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #1 SMP PREEMPT Fri Dec 18 23:47:12 IST 2015
[ 0.083717] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.097142] omap_hwmod: tptc0 using broken dt data from edma-controller
[ 0.097657] omap_hwmod: tptc1 using broken dt data from edma-controller
....
[ 0.429902] reg-fixed-voltage fixedregulator-evm_3v3_sw: Failed to find supply vin
[ 0.430081] reg-fixed-voltage fixedregulator-evm_3v3_sw: Failed to register regulator: -517
[ 0.430100] platform fixedregulator-evm_3v3_sw: Driver reg-fixed-voltage requests probe deferral
[ 0.430347] aic_dvdd: 1800 mV
[ 0.430403] reg-fixed-voltage fixedregulator-aic_dvdd: Failed to find supply vin
[ 0.430577] reg-fixed-voltage fixedregulator-aic_dvdd: Failed to register regulator: -517
[ 0.430596] platform fixedregulator-aic_dvdd: Driver reg-fixed-voltage requests probe deferral
[ 0.430912] vmmcwl_fixed: 1800 mV
[ 0.431430] vtt_fixed: 1350 mV
[ 0.431481] reg-fixed-voltage fixedregulator-vtt: Failed to find supply vin
[ 0.431693] reg-fixed-voltage fixedregulator-vtt: Failed to register regulator: -517
[ 0.431712] platform fixedregulator-vtt: Driver reg-fixed-voltage requests probe deferral
.....
[ 2.489784] omap-sham: probe of 4b101000.sham failed with error -22
.....
[ 2.655206] tlv320aic3x-codec 0-0018: Failed to get supply 'IOVDD': -517
[ 2.661960] tlv320aic3x-codec 0-0018: Failed to request supplies: -517
[ 2.668627] i2c 0-0018: Driver tlv320aic3x-codec requests probe deferral
[ 2.675539] tlv320aic3x-codec 1-0018: Failed to get supply 'IOVDD': -517
[ 2.682294] tlv320aic3x-codec 1-0018: Failed to request supplies: -517
[ 2.688954] i2c 1-0018: Driver tlv320aic3x-codec requests probe deferral
[ 2.695856] tlv320aic3x-codec 1-0019: Failed to get supply 'IOVDD': -517
[ 2.702601] tlv320aic3x-codec 1-0019: Failed to request supplies: -517
[ 2.709265] i2c 1-0019: Driver tlv320aic3x-codec requests probe deferral
[ 2.716155] tlv320aic3x-codec 1-001a: Failed to get supply 'IOVDD': -517
[ 2.722900] tlv320aic3x-codec 1-001a: Failed to request supplies: -517
..............
[ 3.287725] davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver unknown
[ 3.295765] davinci_mdio 48485000.mdio: phy[3]: device 48485000.mdio:03, driver unknown
[ 3.303994] tvp5158 1-0058: Unable to of_probe
...............
[ 16.022614] omap_hwmod: mmu1_dsp1: _wait_target_disable failed
[ 16.034965] omap_hwmod: mmu0_dsp1: _wait_target_disable failed