Hi,
We are testing our custom hardware designed with AM5728 with processor SDK.
LCD is displaying /usr/bin/runWeston: line 39: 692 Segmentation fault weston --idle-time=0 >> /var/log/weston.log 2>&1
The Kernel is hanging with the following messages. Kindly help on this,
2015-10-07 20:22:00: (/home/gtbldadm/processor-sdk-linux-fido-build/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-ne
Initializing /dev/gdbtty0 based on /lib/firmware/dra7-dsp1-fw.xe66 ...
gdb_globalData (local) = 00806000
gdb_globalData (global) = 40806000
Initializing /dev/gdbtty1 based on /lib/firmware/dra7-dsp2-fw.xe66 ...
gdb_globalData (local) = 00806000
gdb_globalData (global) = 41006000
/
Starting Matrix GUI application.
Enabling thermal zones...
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
binutils-dev
binutils
bison-dev
bison
cpp-symlinks
cpp
g++-symlinks
g++
gcc-symlinks
gcc
gdbc6x
gdbserver
gstreamer1.0-libav
libgmp10
libmpc3
libmpfr4
make
parted
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
INIT: Id "O2" respawning too fast: disabled for 5 minutes
[ 303.845708] EXT4-fs (mmcblk0p2): error count since last fsck: 9
[ 303.851670] EXT4-fs (mmcblk0p2): initial error at time 1444248189: ext4_iget:4226: inode 399114: block 1852400175
[ 303.862000] EXT4-fs (mmcblk0p2): last error at time 1452670660: ext4_iget:4207: inode 399114: block 1852400175
INIT: Id "O2" respawning too fast: disabled for 5 minutes