This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with using BlackHawk debbuger

Hi,

I'm using CCSv6 with Blackhawk XDS560v2-USB emulator, on a computer running windows 7 64bit.

When trying to launch a target configuration, I'm getting the following error message:
"Can't generate board data file C:\Users\iplab\AppData\Local\TEXASI~1\CCS\ti\0\0\BrdDat\ccBoard0.dat.
An internal error occurred while expanding the scan-path description."

The same CCXML file is used on multiple computers. It works on some of them and doesn't work on others.

I tried to reinstall the CCSv6 and also tried to update the BlackHawk drivers to the latest, but no luck.

What should I do to solve this issue?