Hi
My hardware is now set BOOT 0100 0000 0101 0110 SPI0 MMC0 UART0, EMAC1. I insert the SD card, after power board can normally start from SD card,After power on, the board also can start from SPI. Board power on can only print eight C,When I remove the SD card Erase SPI,What is the reason? The new production of the same number of cards, no operation, power is the only print eight C.