This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

fail to run DSP application in AM5xx

Hi experts,

I download software from http://software-dl.ti.com/processor-sw/esd/PROCESSOR-SDK-LINUX-AM57X/latest/index_FDS.html , and try something below.

The result is different from http://processors.wiki.ti.com/index.php/Processor_Training:_Multimedia 

root@am57xx-evm:~# copycodectest 123
0x22070: Opening Engine..
MmRpc_create: Error: open failed, name=/dev/rpmsg-dce-dsp
ERROR:decoder_open:111: 0x22070: could not open engine
/home/gtbldadm/processor-sdk-linux-fido-build/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-linux-gnueabi/libdce/3.00.08.02-r0/git/libdce.c:198: dce_ipc_init Error: ERROR: Failed eError == DCE_EOK error val -4/home/gtbldadm/processor-sdk-linux-fido-build/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-linux-gnueabi/libdce/3.00.08.02-r0/git/libdce.c:276: Engine_open Error: ERROR: Failed dce_ipc_init(coreIdx) == DCE_EOK error val -4root@am57xx-evm:~#

I have try following, and it looks weird due to lack of rpmsg-dce-dsp..

root@am57xx-evm:~# ls -l /dev/rpmsg-dce*
crw-rw---- 1 root tisdk 248, 0 Jan 1 1970 /dev/rpmsg-dce
root@am57xx-evm:~#

Is there anything I misunderstand ??

Thanks