This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM1808 connecting external clock against PRU function pin

Guru 15520 points
Other Parts Discussed in Thread: AM1808
Hi,

I have a question about AM1808 pin(A3).

My customer are connecting 48MHz external clock for USB_REFCLKIN against A3 pin of AM1808.
There two type of customer boards. One type of boards doesn't use USB_REFCLKIN, 
so this A3 pin are set to default function(PRU0_R31[17]) but 48MHz clock are still mounted 
and connected to this pin.

They want to know if there are any problem connecting 48MHz clock against PRU0_R31[17] function pin.
Are there any problem like device will get damaged or undesired operation?
By the way, they are not using PRU. best regards, g.f.