Other Parts Discussed in Thread: AM3352
Hi All,
I'm working on am3352 sitara processor based custom designed board using SDK-8.0
The am335x UART0 is connected to GSM module with Hardware flow control
I've configured in Device tree to enable Hard ware flow control as below
uart0_pins: pinmux_uart0_pins {
pinctrl-single,pins = <
0x168 (PIN_INPUT | MUX_MODE0) /* uart0_ctsn.uart0_ctsn */
0x16C (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* uart0_rtsn.uart0_rtsn */
0x170 (PIN_INPUT_PULLUP | MUX_MODE0) /* uart0_rxd.uart0_rxd */
0x174 (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* uart0_txd.uart0_txd */
>;
};
The hardware flow control is not working(Not toggling RTS and CTS) as expected, is i'm missing any configurations or setting ?
Please suggest ASAP
Thanks and Regards,
Thiru N