This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omap-resizer module

Hello,

I am getting below kernel messages on Beagleboard. Does these errors, related to "omap-resizer" module make any sense to anyone?

[  638.577087] omap-resizer: Device is opened in blocking mode

[  638.968475] Unable to handle kernel NULL pointer dereference at virtual address 00000008

[  638.968505] pgd = ce574000

[  638.968505] [00000008] *pgd=8f05b031, *pte=00000000, *ppte=00000000

[  638.968536] Internal error: Oops: 17 [#1] PREEMPT

[  638.968536] Modules linked in: omaplfb pvrsrvkm v4l2_common videodev v4l1_compat v4l2_int_device omap_resizer isp_mod iovmm iommu videobuf_dma_sg videobuf

[  638.968627] CPU: 0    Not tainted  (2.6.29-omap1 #1)

[  638.968780] PC is at isp_set_callback+0x16c/0x190 [isp_mod]

[  638.968841] LR is at isp_set_callback+0x68/0x190 [isp_mod]

[  638.968872] pc : [<bf06ad08>]    lr : [<bf06ac04>]    psr: 80000013

[  638.968872] sp : ce53bdd0  ip : ce53bdd0  fp : ce53bdf4

[  638.968872] r10: 00000003  r9 : ce53a000  r8 : bf093f00

[  638.968902] r7 : 00000000  r6 : 00000000  r5 : 00000003  r4 : a0000013

[  638.968902] r3 : 01000000  r2 : ce53a000  r1 : 00000000  r0 : 00000000

[  638.968933] Flags: Nzcv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

[  638.968933] Control: 10c5387d  Table: 8e574019  DAC: 00000015

[  638.968963] Process mud (pid: 2296, stack limit = 0xce53a2e8)

[  638.968963] Stack: (0xce53bdd0 to 0xce53c000)

[  638.968994] bdc0:                                     c005ac4c cf10a400 d80bd000 ce4fd780

[  638.969024] bde0: cf1ed700 ce4fd880 ce53be24 ce53bdf8 bf09334c bf06aba8 cf1ed700 00000000

Thanks!