Other Parts Discussed in Thread: AM3359
Hi,
I would like to know if there's a way I can check the current clock values for each peripheral, as well as PLLs in kernel space.
Regards,
Guilherme
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AM3359
Hi,
I would like to know if there's a way I can check the current clock values for each peripheral, as well as PLLs in kernel space.
Regards,
Guilherme
Along similar lines, omapconf has a "show dpll" command that produces an output like this:
root@am335x-evm:~# omapconf show dpll
OMAPCONF (rev v1.71-11-g576b01f built Mon Jul 6 15:54:36 EDT 2015)
HW Platform:
Generic AM33XX (Flattened Device Tree)
AM3359 ES2.1 GP Device (UNKNOWN performance ZCZ package (1.0GHz))
Error: I2C Read failed
Error: I2C Read failed
Error: I2C Read failed
Error: I2C Read failed
UNKNOWN POWER IC
Error: I2C Read failed
UNKNOWN AUDIO IC
SW Build Details:
Build:
Version: _____ _____ _ _
Kernel:
Version: 3.14.43-g875c69b
Author: gtbldadm@ubuntu-12
Toolchain: gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03)
Type: #1
Date: Mon Jul 6 16:00:11 EDT 2015
|--------------------------------------------|
| DPLL Configuration | DPLL_PER |
|--------------------------------------------|
| Status | Locked |
| | |
| Mode | Lock |
| Automatic Control | Not Supported |
| LPST = Low-Power STop | |
| LPBP = Low-Power ByPass | |
| FRBP = Fast-Relock ByPass | |
| MNBP = MN ByPass | |
| | |
| Sigma-Delta Divider | 4 |
| SELFREQDCO | 0 |
| | |
| Ref. Frequency (MHz) | 24.000 |
| M Multiplier Factor | 960 |
| N Divider Factor | 23 |
| Lock Frequency (MHz) | 960 |
| | |
| CLKOUT Output | |
| Status | Enabled |
| Clock Divider | 5 |
| Clock Speed (MHz) | 192 |
| | |
| CLK_DCO_LDO Output | |
| Status | Enabled |
| Clock Speed (MHz) | 960 |
| | |
|--------------------------------------------|
|---------------------------------------------------------------------------------------------|
| DPLL Configuration | DPLL_CORE | DPLL_MPU | DPLL_DDR | DPLL_DISP |
|---------------------------------------------------------------------------------------------|
| Status | Locked | Locked | Locked | Locked |
| | | | | |
| Mode | Lock | Lock | Lock | Lock |
| Automatic Control | Not Supported | Not Supported | Not Supported | Not Supported |
| LPBP = Low-Power ByPass | | | | |
| FRBP = Fast-Relock ByPass | | | | |
| MNBP = MN ByPass | | | | |
| Low-Power Mode | Disabled | Disabled | Disabled | Disabled |
| | | | | |
| Automatic Recalibration | Disabled | Disabled | Disabled | Disabled |
| Clock Ramping during Relock | Disabled | Disabled | Disabled | Disabled |
| Ramping Rate (x REFCLK(s)) | 2 | 2 | 2 | 2 |
| Ramping Levels | No Ramp | No Ramp | No Ramp | No Ramp |
| | | | | |
| Bypass Clock | CLKINP | CLKINP | CLKINP | CLKINP |
| Bypass Clock Divider | | | | |
| REGM4XEN Mode | Disabled | Disabled | Disabled | Disabled |
| | | | | |
| Ref. Frequency (MHz) | 24.000 | 24.000 | 24.000 | 24.000 |
| M Multiplier Factor | 1000 | 25 | 303 | 5 |
| N Divider Factor | 23 | 1 | 23 | 1 |
| Lock Frequency (MHz) | 1000 | 300 | 303 | 60 |
| | | | | |
| M2 Output | | | | |
| Status | | Enabled | Enabled | Enabled |
| Clock Divider | | 1 | 1 | 1 |
| Clock Speed (MHz) | | 300 | 303 | 60 |
| | | | | |
| CLK_DCO_LDO Output | | | | |
| Status | Gated | | | |
| Clock Speed (MHz) | 2000 | | | |
| | | | | |
| | | | | |
| M4 Output | | | | |
| Status | Enabled | | | |
| Clock Divider | 10 | | | |
| Clock Speed (MHz) | 200 | | | |
| | | | | |
| M5 Output | | | | |
| Status | Enabled | | | |
| Clock Divider | 8 | | | |
| Clock Speed (MHz) | 250 | | | |
| | | | | |
| M6 Output | | | | |
| Status | Gated | | | |
| Clock Divider | 4 | | | |
| Clock Speed (MHz) | 500 | | | |
|---------------------------------------------------------------------------------------------|