in our project we got video data from DM6467 PCI interface then the DSP process the video data. the video data rate 50MB/s, when we use the 594Mhz DM6467 it is work! now, we go to DM6467T 1GHz , it does not work well. when we setup the DM6467T to 726MHz ,it work well again. In my opinion, it is the DDR bandwidth problem, but when I set these Bus Master Priority Control 0 (like 0x01C4003C MSTPRI0 ) The problem remains unresolved.
how can we do to use the DM6467T ??