I need to build Qt in exactly the same way it was build for this old version of the SDK to do static code analysis using CodeSonar - this static analysis tool "snoops" the build to "understand" the code it is analyzing.
One would think that this configuration should be exactly known to someone at TI, because they had to build it to include it in the SDK.
I am familiar with the general mechanics of doing so, but to duplicate the version in the SDK, I would need the mkspec and the string passed to ./configure that was used to build the library for the SDK. Help would be appreciated.
At some point we plan to update to the latest and greatest version of the SDK, but at this point in this project, that is not in the cards, so pointing me to how to build the latest version will not likely be too helpful.
Thanks in Advance,
marion