Hi,
I am trying some ADPLLS setting to reduce LCDC Clock jitters.
And then I have a question about DPLL DISP(ADPLLS) register setting.
There are the following two cases:
1)CLK24MHz, M=891, N=15, M2=9 =>148.5MHz => OK
CM_DIV_M2_DPLL_DISP(0x44E004A4) : 0x00000309
CM_CLKSEL_DPLL_DISP(0x44e00454) : 0x00037B0F
CM_IDLEST_DPLL_DISP(0x44E00448) : 0x1 ※Lock
2)CLK24MHz, M=900, N=15, M2=10 => NG
CM_DIV_M2_DPLL_DISP(0x44E004A4) : 0x0000030A
CM_CLKSEL_DPLL_DISP(0x44e00454) : 0x0003DE0F
CM_IDLEST_DPLL_DISP(0x44E00448) : 0x0 ※Unlock
#I have confirmed this on AM335x EVM.
Form TRM, ADPLLS can multiply up to 2-GHz maximum. So 2) should be OK. But It becomes Unlock.
Why not? ADPLLS DCO frequency is slower than 2GHz?
Best Regards,
Taka