Hi,
I am using OMAP 35x EVM rev G. board, with PSP 2.01.03.11. I connect the DVI output to my SVGA display (1280 x 1024 60Hz) and using fbset -xres 1280 and fbset -yres 1024. Then I run interface, but the output only occupies a quarter of my SVGA display. Did I setup OMAP correctly? Or there are something missing? Thanks.
Annie